You are here: Understanding KAS > Motion Concepts > PLCopen > Axes Group Parameters

Axes Group Parameters

The table below is a list of Boolean parameters currently supported. These parameters are read and written by the function blocks MC_GrpReadBoolPar and MC_GrpWriteBoolPar.

Parameter ID Name R/W Description
MC_GRP_PARAM_IGNORE_AXIS_ESTOP 1000 Ignore Axis EStop Read/Write Controls whether the axes group will continue performing motion if one of the member axes is experiencing an Estop. A value of FALSE indicates that the axes group should enter an Estop state if a member axis enters the Estop state. A value of TRUE indicates that the axes group should continue performing motion.
MC_GRP_PARAM_AXIS_ESTOP_ACTIVE 1001 Axis EStop Active Read Only This Read-only parameter will be asserted TRUE whenever an axis in the group is experiencing an axis Estop Error. When there are no axis Estop Errors present on the axes in a group, this parameter will be set to FALSE.

The table below is a list of non-Boolean parameters currently supported. These parameters are read and written by the function blocks MC_GrpReadParam and MC_GrpWriteParam.

Parameter ID Name R/W Description
MC_GRP_PARAM_CIRCLE_TOLERANCE 2000 Command Velocity Read/Write This parameter controls how large an error will be acceptable when constructing circles using circle mode MC_CIRC_MODE_CENTER. A value of zero will default to the 1 part in 100,000 tolerance. For more information see Precision Requirements for Circular Move Input Parameters.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™